This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champs,
In my customer's application, high resolution period and high resolution duty cycle will be used simultaneously. And they found there were some jitter on the ePWMxA's output.
You can see the scope capture as follows. The yellow waveform is ePWM1A output, and the blue one is ePWM3A output.
And also, if EPwm1Regs.HRPCTL.bit.HRPE was set to zero, the jitter will be gone.
So the question is whether high resolution period and high resolution duty cycle can be used simultaneously?
Thanks.
Regards,
Young
According to this:
HRPWM for for hi-res duty and period control in up-down count (symmetric) mode - C2000 microcontrollers...
It is possible but you must follow this:
// Disable TBCLKSYNC EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; //Write To CMP, TBPRD, TBPHS registers. (*ePWM[j]).TBCTL.bit.PRDLD = TB_SHADOW; // set Shadow load (*ePWM[j]).TBPRD = period; // PWM frequency = 1/(2*TBPRD) (*ePWM[j]).CMPA.half.CMPA = period / 2; // set duty 50% initially (*ePWM[j]).CMPA.half.CMPAHR = (0 << 8); // initialize HRPWM extension (*ePWM[j]).TBPHS.all = 0; //Configure modes, clock dividers and action qualifier (*ePWM[j]).TBCTR = 0; (*ePWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down count mode (*ePWM[j]).TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE; (*ePWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV1; (*ePWM[j]).TBCTL.bit.CLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT (*ePWM[j]).TBCTL.bit.FREE_SOFT = 00; (*ePWM[j]).CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // LOAD CMPA on CTR = 0 (*ePWM[j]).CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; (*ePWM[j]).CMPCTL.bit.SHDWAMODE = CC_SHADOW; (*ePWM[j]).CMPCTL.bit.SHDWBMODE = CC_SHADOW; (*ePWM[j]).AQCTLA.bit.CAU = AQ_SET; (*ePWM[j]).AQCTLA.bit.CAD = AQ_CLEAR; (*ePWM[j]).AQCTLB.bit.ZRO = AQ_SET (*ePWM[j]).AQCTLB.bit.PRD = AQ_CLEAR; //Configure HRPWM registers EALLOW; (*ePWM[j]).HRCNFG.all = 0x0; (*ePWM[j]).HRCNFG.bit.EDGMODE = HR_BEP; // MEP control on both edges (*ePWM[j]).HRCNFG.bit.CTLMODE = HR_CMP; // CMPAHR and TBPRDHR HR control (*ePWM[j]).HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD; // load on CTR = 0 and CTR = TBPRD (*ePWM[j]).HRCNFG.bit.AUTOCONV = 1; // Enable autoconversion (*ePWM[j]).HRPCTL.bit.HRPE = 1; // Turn on high-resolution period control //set TBCTL[PHSEN] = 1 (*ePWM[j]).TBCTL.bit.PHSEN = 1; //set HRPCTL[TBPHSHRLOADE] = 1 (*ePWM[j]).HRPCTL.bit.TBPHSHRLOADE = 1; //Do the same to all other PWM modules … //Enable TBCLKSYNC SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; //Perform a software sync EPwm1Regs.TBCTL.bit.SWFSYNC = 1;
Hi Nima,
Customer revise the code accordingly, but the issue still exists. Would you kindly help to review the code as follows?
void HRPWM_TG_Config(period)
{ Uint16 j; // // ePWM channel register configuration with HRPWM // ePWMxA toggle low/high with MEP control on Rising edge // // Disable TBCLKSYNC EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; for(j=1; j<PWM_CH; j++) { //Write To CMP, TBPRD, TBPHS registers. (*ePWM[j]).TBCTL.bit.PRDLD = TB_SHADOW; // set Shadow load (*ePWM[j]).TBPRD = period; // PWM frequency = 1/(2*TBPRD) (*ePWM[j]).TBPRDHR = (1 << 8); // PWM frequency = 1/(2*TBPRD) (*ePWM[j]).CMPA.bit.CMPA = period/2; // set duty 50% initially (*ePWM[j]).CMPA.bit.CMPAHR = (1 << 8); // initialize HRPWM extension (*ePWM[j]).TBPHS.all = 0; //Configure modes, clock dividers and action qualifier (*ePWM[j]).TBCTR = 0; (*ePWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Select up-down count mode (*ePWM[j]).TBCTL.bit.SYNCOSEL = TB_SYNC_IN; (*ePWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV1; (*ePWM[j]).TBCTL.bit.CLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT (*ePWM[j]).TBCTL.bit.FREE_SOFT = 0x00; (*ePWM[j]).CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // LOAD CMPA on CTR = 0 (*ePWM[j]).CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; (*ePWM[j]).CMPCTL.bit.SHDWAMODE = CC_SHADOW; (*ePWM[j]).CMPCTL.bit.SHDWBMODE = CC_SHADOW; (*ePWM[j]).AQCTLA.bit.CAU = AQ_SET; (*ePWM[j]).AQCTLA.bit.CAD = AQ_CLEAR; // (*ePWM[j]).AQCTLB.bit.ZRO = AQ_SET; // (*ePWM[j]).AQCTLB.bit.PRD = AQ_CLEAR; //added (*ePWM[j]).DBCTL.bit.OUT_MODE = 0x2;//S1=1,S0=1 (*ePWM[j]).DBCTL.bit.POLSEL = 0x0;//S3=1,S2=0 (*ePWM[j]).DBCTL.bit.IN_MODE = 0x2;//S5=1,S4=0 (*ePWM[j]).DBRED.bit.DBRED = 20;//DC_DB_TIME_200NS; //Configure HRPWM registers EALLOW; (*ePWM[j]).HRCNFG.all = 0x0;//// (*ePWM[j]).HRCNFG.bit.HRLOAD = HR_CTR_ZERO; (*ePWM[j]).HRCNFG.bit.CTLMODE = HR_CMP; (*ePWM[j]).HRCNFG.bit.EDGMODE = 0x2;//control of both edges (TBPHSHR or TBPRDHR) (*ePWM[j]).HRCNFG.bit.AUTOCONV = 1; // Enable autoconversion (*ePWM[j]).HRPCTL.bit.TBPHSHRLOADE = 1; (*ePWM[j]).HRPCTL.bit.HRPE=1; // Turn on high-resolution period control. EDIS; } //Enable TBCLKSYNC EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; //Perform a software sync EPwm1Regs.TBCTL.bit.SWFSYNC = 1; }
Thanks.
Young
Hello guys, I am experiencing the same issue with a TMS320F280049M. I am following the sample code from post
In any case, doing UP_DOWN or UP only count, I get jitters with a size of 1 count (10nsec in my case per coarse step)... Any solution so far?
Best regards,
Alberto
Yes the problem in the code is:
(*ePWM[j]).HRCNFG.bit.HRLOAD = HR_CTR_ZERO_PRD;
// load on CTR = 0 and CTR = TBPRD
They MUST load on both ZERO and PERIOD.
If they dont they will face that issue.
TMS320F280049: PWM pin output signal is not stable when period and CMPA are fixed - C2000 microcontrollers...
The link above is the same issue.
Hi Nima,
You can refer the project from the following link, and unzip this file to C:\TI\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Cpu1.
Many thanks,
Young
Found the issue. In the HRPWM config function the code was not setting EDGEMODE to both edges. In the comment, it said "both edges" however in the customer code you sent me, the value used was "2". If you change that to "3" which is both edges as mentioned in the TRM, you see that the jitter will disappear.
So here is what I changed in the code: