This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
The HVPM Sensorless from controsuit are just has one parameter(LS), stator inductance. If the motor is IPM, that Ls-q and Ls-d are provided and different, how to configure this parameter in this settings? Thanks...
// Define the electrical motor parametes (Estun Servomotor)
#define RS 2.35 // Stator resistance (ohm)
#define RR // Rotor resistance (ohm)
#define LS 0.0065 // Stator inductance (H)
#define LR // Rotor inductance (H)
#define LM // Magnatizing inductance (H)
#define POLES 8 // Number of poles
Hello,
I consider this thread as closed for now. If you have further queries, disregard the closure and reply back in this thread or refer to this thread and post your queries if you reply too late.