Other Parts Discussed in Thread: UNIFLASH
I created a batch script for the TMS320F28379D dual core microcontroller using the Standalone Command Line generator in Uniflash v4.3.1.1835. The programming of CPU1 using the resulting dslite.bat file is successful. The programming of CPU2 fails when calling the generated batch script file for CPU2. I have included the output of the batch file below. Is there a way to utilize the generated batch script from the Uniflash Command Line option to program CPU2?
many thanks for your response
Executing default command:
> dslite --mode flash -c user_files/configs/f28379d.ccxml -l user_files/settings
/generated.ufsettings -e -f "user_files/images/cpu2_release_1.out"
-n 1
DSLite version 8.1.0.1275
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: IcePick_C_0
Loaded FPGA Image: C:\Software\uniflash_windows_64\ccs_base\common\uscif\dtc_top
.jbc
Executing Startup Scripts: IcePick_C_0
Initializing: C28xx_CPU1
Executing Startup Scripts: C28xx_CPU1
Initializing: CPU1_CLA1
Executing Startup Scripts: CPU1_CLA1
Initializing: C28xx_CPU2
Executing Startup Scripts: C28xx_CPU2
Initializing: CPU2_CLA1
Executing Startup Scripts: CPU2_CLA1
Connecting...
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
info: C28xx_CPU1: If erase/program (E/P) operation is being done on one core, th
e other core should not execute from shared-RAM (SR) as they are used for the E/
P code. Also, CPU1 will be halted to determine SR ownership for the CPU which w
ill run the Flash Plugin code, after which CPU1 will be set to run its applicati
on. User code execution from SR could commence after both flash banks are progra
mmed.
Loading Program: user_files/images/cpu2_release_1.out
Preparing ...
.text: 0 of 9326 at 0x8928c
error: CPU1_CLA1: File Loader: Verification failed: Values at address 0x0008928C
do not match Please verify target memory and memory map.
Finished
Failed: File: user_files/images/cpu2_release_1.out: a data verificat
ion error occurred, file load failed.