Hi,
I am working with a TMS20f2812 dsp board, which has a DAC connected to XINTF bus. I want to see some variable in the DSP code via this DAC output in an oscilloscope. How is it possible to put these signals on the XINTF bus? These are non critical signals, and used for debugging purpose. Can I use a UOUT command? What is the address of XD register for putting the signal?
Thanks for the help,
Anandarup Das