Hello,
What are the restrictions on EPWMxB when High Resolution is being used. If I generate two PWM signals EPWMxA and EPWMxB as complementary waveforms will EPWMxB be high resolution as well?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What are the restrictions on EPWMxB when High Resolution is being used. If I generate two PWM signals EPWMxA and EPWMxB as complementary waveforms will EPWMxB be high resolution as well?
Thanks
user4997907,
The B signal path of an ePWM channel can generate a high-resolution output by either swapping the A and B outputs (the high-resolution signal will appear on ePWMxB instead of ePWMxA) or by outputting an inverted version of the high-resolution ePWMxA signal on the ePWMxB pin.
Stated another way, if you use the dead-band sub-module only one channel of the PWM can be high-resolution not both.
If you don't need dead-band control and only want a high-resolution complementary PWM signal this can be done with "HRCNFG.SELOUTB = 1".
Regards,
Cody