Part Number: TMDSDOCK28335
Tool/software: Code Composer Studio
Sir,
I am trying to run the boost converter in closed loop voltage control mode using DF22 controller. By placing breakpoints at various lines I have observed that the program is entering into ILLEGAL_ISR(void) just before or while executing the line
u2k = DCL_runDF22_C2(&controller2, ek);
What are the probable reasons behind this and how to overcome this problem ?
I am attaching the complete code of main.c, please go through it and suggest any modifications if necessary.
//########################################################################### // $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $ // $Release Date: November 1, 2016 $ // $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include "DCL.h" // #include "F2833x_Device.h" // #include "F2833x_Examples.h" // #include "F2833x_GlobalPrototypes.h" #include "DCLF32.h" #include "DCL_fdlog.h" // Prototype statements for functions found within this file. __interrupt void adc_isr(void); void InitEPwm2Example(void); #define EPWM1_TIMER_TBPRD 1500 // Period register #define EPWM1_CMPA 1050 //INPUT DATA #define DATA_LENGTH 1601 #pragma DATA_SECTION(e_array, "PDataLogSection") float e_array[DATA_LENGTH]; FDLOG eBuf = FDLOG_DEFAULTS; // full controller results #pragma DATA_SECTION(u1_array, "QDataLogSection") float u1_array[DATA_LENGTH]; FDLOG u1Buf = FDLOG_DEFAULTS; // pre-computed controller results #pragma DATA_SECTION(u2_array, "RDataLogSection") float u2_array[DATA_LENGTH]; FDLOG u2Buf = FDLOG_DEFAULTS; // controller difference data #pragma DATA_SECTION(d_array, "SDataLogSection") float d_array[DATA_LENGTH]; FDLOG dBuf = FDLOG_DEFAULTS; // extern interrupt void control_Isr(void); __interrupt void adc_isr(void); // global variables long IdleLoopCount = 0; long IsrCount = 0; float u1k; float u2k; float dk; float upperLim; float lowerLim; uint16_t v; DCL_DF22 controller1 = DF22_DEFAULTS; DCL_DF22 controller2 = DF22_DEFAULTS; int vadc=0; // FDLOG eBUf = FDLOG_DEFAULTS; int out=0; // Global variables used in this example: // Uint16 ConversionCount; float rk = 0.4199f * 4096; float ek; float yk; main() { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); DINT; InitEPwm2Gpio(); /*.............................ADC_BLOCK..........................*/ EALLOW; #if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz #endif #if (CPU_FRQ_100MHZ) #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz #endif EDIS; // Define ADCCLK clock frequency ( less than or equal to 25 MHz ) // Assuming InitSysCtrl() has set SYSCLKOUT to 150 MHz EALLOW; SysCtrlRegs.HISPCP.all = ADC_MODCLK; // High Speed Periphal clock set to 25 MHz EDIS; // Step 2. Initialize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; InitEPwm2Example(); EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS; InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected register PieVectTable.ADCINT = &adc_isr; PieVectTable.TINT0 = &adc_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example InitAdc(); // For this example, init the ADC // Step 5. User specific code, enable interrupts: // Enable ADCINT in PIE PieCtrlRegs.PIEIER1.bit.INTx6 = 1; IER |= M_INT1; // Enable CPU Interrupt 1 EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM v = 0; // Configure ADC AdcRegs.ADCTRL1.bit.ACQ_PS = 0x2; AdcRegs.ADCTRL1.bit.CPS = 0x1; //AdcRegs.ADCTRL3.bit.ADCCLKPS = 0x1; AdcRegs.ADCMAXCONV.all = 0x0000; // Setup 2 conv's on SEQ1 AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; // Setup ADCINA0 as 1st SEQ1 conv. //AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1; // Setup ADCINA1 as 2nd SEQ1 conv. AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;// Enable SOCA from ePWM to start SEQ1 AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS) AdcRegs.ADCTRL3.bit.SMODE_SEL = 1; // Assumes ePWM1 clock is already enabled in InitSysCtrl(); EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group EPwm1Regs.ETSEL.bit.SOCASEL = 2; // Select SOC from from CPMA on upcount EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event EPwm1Regs.CMPA.half.CMPA = 0x08FF; // Set compare A value EPwm1Regs.TBPRD = 0x0FFF; // Set period for ePWM1 EPwm1Regs.TBCTL.bit.SYNCOSEL = 0x01; EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start // Wait for ADC interrupt /* for(;;) { } */ /*............... CONTROLLER SECTION....................*/ // configure CPU timer 0 InitCpuTimers(); ConfigCpuTimer(&CpuTimer0, 90.0, 1.0e+03); // initialise data arrays DCL_initLog(&eBuf, e_array, DATA_LENGTH); DCL_initLog(&u1Buf, u1_array, DATA_LENGTH); DCL_initLog(&u2Buf, u2_array, DATA_LENGTH); DCL_initLog(&dBuf, d_array, DATA_LENGTH); DCL_clearLog(&u1Buf); DCL_clearLog(&u2Buf); DCL_fillLog(&dBuf, 1.234567f); // initialise full controller controller1.a1 = -0.5075f; controller1.a2 = -0.4925f; controller1.b0 = 0.01614f; controller1.b1 = 3.84e-5f; controller1.b2 = -0.0161f; // Initialize Pre-computed controller controller2.a1 = controller1.a1; controller2.a2 = controller1.a2; controller2.b0 = controller1.b0; controller2.b1 = controller1.b1; controller2.b2 = controller1.b2; // clamp limits upperLim = 4096.0f; lowerLim = 0.0f; // enable interrupts PieCtrlRegs.PIEIER1.bit.INTx7 = 1; IER |= M_INT1; EINT; StartCpuTimer0(); // idle loop while(1) { IdleLoopCount++; } } // end of main __interrupt void adc_isr(void) { /*.....................................CONTROL BLOCK.............................*/ // clear timer flag & acknowledge interrupt CpuTimer0Regs.TCR.bit.TIF = 1; PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; yk = ((float) AdcMirror.ADCRESULT0); ek = rk - yk; // run pre-computed controller u2k = DCL_runDF22_C2(&controller2, ek); out = (int) u2k; EPwm2Regs.CMPA.half.CMPA = (out) ; EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Set PWM1A on Zero EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; EPwm2Regs.AQCTLB.bit.CAU = AQ_SET; // Set PWM1B on Zero initialize... EPwm2Regs.AQCTLB.bit.CAD = AQ_CLEAR; // Clear INT flag for this timer EPwm2Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; v = DCL_runClamp_C1(&u2k, upperLim, lowerLim); if (0 == v) { DCL_runDF22_C3(&controller2, ek, u2k); } // store results DCL_writeLog(&u1Buf, u1k); DCL_writeLog(&u2Buf, u2k); DCL_writeLog(&dBuf, dk); IsrCount++; if(IdleLoopCount==0) { if(v == DATA_LENGTH) { v = 0; IdleLoopCount=1; } else { vadc = (AdcRegs.ADCRESULT0 >>4) ; e_array[v]= vadc; v++; } } // Reinitialize for next ADC sequence AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1 AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE return; } void InitEPwm2Example() { // Setup TBCLK EPwm2Regs.TBPRD = 750; // Set timer period 801 TBCLKs EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0 EPwm2Regs.TBCTR = 0x0000; // Clear counter // Set Compare values EPwm2Regs.CMPA.half.CMPA = out; // Setup counter mode EPwm2Regs.TBCTL.bit.CTRMODE = 0; // Count up EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; EPwm2Regs.TBCTL.bit.SYNCOSEL = 0x00; // Setup shadowing EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Set actions EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on event A, up count EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM2A on event A, down count }
Waiting for the solution.
Regards,
Soumya.