This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28035: Moving from assembler to C for CLA

Part Number: TMS320F28035

Tool/software: TI C/C++ Compiler

Hello.

I am taking over an old C2000 project that uses Makefiles.

The original programmer was using Cygwin to build the project. 

I have recreated the same environment on my computer and got everything work. So I am good to move on.

At the same time I wanted to get everything into CCS8 basically Eclipse. I got that working too. Everything is good after getting some help from this forum.

Now I want to move away from some assembler files CLA related. 

Ki give me a link for C2000 Ware. It seems to be the right direction.

Because I don't have any history with C2000 compiler, I wanted to confirm that those assemblers were developed when there was no library available, not for speed reasons. And I am able to use the latest library to replace them.

Just wanted to have a general feeling to see if what I am trying to makes sense.

Thanks

Paul

  • Hi Paul,

    That is likely the situation. The CLA initially didn't have C compiler support. Now it does. And we also offer a CLA math library which is in lieu of the math.h C library which is not support on the CLA.

    Hope this help,
    sal
  • Thanks Sal

    That answers my question.

    For now I will keep the assembly code ASIS because we have very strict code validation procedure here.

    But I will give it a try as a branch when I have time.

    Paul