This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As shown in the F28004x datasheet, why are there 2 values for the erase time? My customer got the challenge in F28035 that the erase time is too long, as shown in Table 5-14, which up to 2s per sector. I hope in F28004x this can be improved, but I don't understand what 25 cycles and 20K cycles refer to. And which one is the right one to compare with 2s for F28035. Highly appreciate with your comment.
Aki,
The 25 and 20K cycles refers to the number of times the device has been erased and programmed. When the flash is new, it erases faster. After you erase and re-flash the device multiple times, it starts to take longer to erase.
Regards,
David
Aki Li said:
How about the erase time for the cycle times between 25 and 20K, so it will increase from 15ms to 120ms?
I would expect yes, the typical erase time will increase from 15ms to 120ms between 25 and 20K cycles.
Aki Li said:
And one more question for the max value, I saw the comment in F28035, "Maximum flash parameter mentioned are for the first 100 program and erase cycles", so it is also the case for F28004x?
David,
Customer is asking for the erase time if the erase cycle>100? Do we have this parameter?
Aki,
Thank you for bringing this up. I filed a ticket for Datasheet update to include an explanation for the Erase time at 25 and 20K cycles. That will help users.
Please open a new thread for F28035 erase time question so that corresponding expert can be assigned for the post to help you.
Thanks and regards,
Vamsi