This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: How to understand the erase time of flash parameters ?

Part Number: TMS320F280049

As shown in the F28004x datasheet, why are there 2 values for the erase time?  My customer got the challenge in F28035 that the erase time is too long, as shown in Table 5-14, which up to 2s per sector. I hope in F28004x this can be improved, but I don't understand what 25 cycles and 20K cycles refer to. And which one is the right one to compare with 2s for F28035.  Highly appreciate with your comment.