This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INSTASPINFOCMOTORWAREGUI: Which device could support Motorware lab11b?

Part Number: INSTASPINFOCMOTORWAREGUI
Other Parts Discussed in Thread: MOTORWARE

Hi ,

My customer use F28069 control card evaluate vibrate compensation based on Motorware lab11b example.

The performance is very good. They would kick off a project using the code soon. Prefer to use F28034.

I aware that there are some code programmed in ROM for Motorware. 

Can I port it to F28034 directly or only could be migrated to InstaSPIN supported device, like F2806x, F28004xC and F28002xC?

Thanks a lot.