This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-1000: What is the meaning of AC_FREQ in the settings.h. file?

Part Number: TIDM-1000

Tool/software: Code Composer Studio

Hi,What is the meaning of AC_FREQ in the settings.h. file?What is the role in the program?If the input frequency is increased to 200HZ, is this parameter to be changed to 200?

Looking forward to your help, thank you!
  • Hi,

    This parameter is not used in the reference design and we will update the software in the next release. You can ignore it and you don't need to change anything in the code. However, for this reference design, we only tested the 50Hz and 60Hz conditions. The tests under other conditions which are not covered in the user guide should be done very carefully by the users.

    Regards,

    Chen