This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: How to change the AC_FREQ in the pfc3phviennaz-settings.h file?

Part Number: TMS320F28379D
Other Parts Discussed in Thread: SYSCONFIG

The AC_FREQ became 60Hz when i rebuild the project of main.cfg, how to modify the parameter?

--

Thanks & Regards

Yale

  • Hi Yale,

    I have checked on the main.sysconfig, I see 60Hz is kept fixed and can be seen in the generated files. 

    I dont think 50Hz option is enabled in sysconfig yet. I can check with other experts and get back to you soon. Are you trying to run any higher frequency range like 350Hz-400Hz?

    Best Regards,

    Uttam

  • +++ adding more information

    Yale, you can use non-power suite project to change the system frequency. 

    Let me know if you still need some help on it.

    Best,

    Uttam