This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I would like to use F28379 launchpad to communication with LTC6811 demo board via SPI. I would like to configure the SPI clock line to be active high when there is no SPI communication.
Here is what I want:
However, here is what I get:
Do you know how to configure SPI clock line to be the one LTC6811 requires?
Thanks
Fei
Hi Haizhu,
Thanks for your reply. I look at SPI clocking schemes in the technical reference manual as you mentioned, but I didn't see anything about how to configure the SPI clock line to be active high when idle. Can you be more specific?
Fei
Hi,
As Haizhu Li mentioned, please refer to the chapter SPI Clocking Schemes (18.3.6).
If you are using C2000ware driverlib, refer to the SPI_TransferProtocol parameter used in SPI_setConfig function
Regards,
veena