This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
when i test the 28035+DRV8305 to control the BLDC motor. there are some problem to issue.
i use the SPI configure the DRV8305 . when i choose the 3PWM model, the GHA Output is right. but when i choose 6PWM model ,the GHA Output is wrong. the Output Value is like add 24V .
and when i choose 6pwm model. if INA is low and ILA is also low,the GHA is high as 24V the GLA is low. why the GHA output is 24V?
Please refer to the PWM configuration in "PM_Sensorless" project in controlSUITE even though the project is for DRV8301, you need to configure the PWM of C2000 to the complementary mode enabling dead band for 6-pwm mode of DRV8305.
C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\PM_Sensorless