This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Default state (internal Pullup/Pulldown) of GPIO pin

Part Number: TMS320F28335

The data sheet of the MCU says 

" All GPIO pins are I/O/Z and have an internal pullup, which can be selectively enabled/disabled on a per-pin basis.

This feature only applies to the GPIO pins. The pullups on GPIO0-GPIO11 pins are not enabled at reset. The pullups on GPIO12-GPIO34 are enabled upon reset."

I did not find any details on default pullup/down status at reset for GPIO35-87. 

Could you please let me know the default state of these GPIO pins.

-Manish