This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Maximum SPI Clock Rate in Slave Mode using High Speed GPIO

Part Number: TMS320F28379D

This question is actually for F2837x and F28004x families of devices. What is the maximum SPI clock rate supported in Slave mode. If I read the datasheet(s), it says 4 LPSYSCLK cycles. I interpret that to be:

  • F2837x: 50 MHz
  • F2807x: 30 MHz
  • F28004x: 25 MHz

Are there any other limitations that I should know about which would restrict the SPI clock rate further in slave mode.

Thanks,

Stuart

  • Stuart,

    • F2837x: 50 MHz
    • F2807x: 30 MHz
    • F28004x: 25 MHz

    Information you have tabulated is indeed correct. Generally the trace lengths of the connections between master and slave can limit the SPI clock rate.

    Regards,

    Manoj