Part Number: TMS320F28035
Hi,
I want to implement sensorless FOC for two BLDC motors using Simulink. But in addition to that I also need to implement fail safe algorithm. Based on some external sensor input the algorithm logic is written and feed back of current, voltage and temperature of both the motors also should be calculated for fail safe operation. I am very new to this field, Please suggest whether TI C2000 launchpad duel motor for FOC will support my requirement or suggest me any other alternative hardware that will support my model.
I had attached my simulink model workflow as an image file
, where I just want to control the orientation of both the motors with the feedback obtained from the running motor and other external sensor.
Thank you