This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to ask, how many microamperes is current sinking on ADC input pins of TMS320F28379D?
When I measured sinking current, some analog input pins (e.g. ADCINA3, ADCINB3) have zero sink current and some ones (e.g. ADCINA1, ADCINB1) have sink current of tens of microampers.
This current sinking affects previous circuits and then measurement is inaccurate.
There is the sink current on the ADC input pin even when ADC module is disabled (ADC power down and ADC module clock is gated-off).
Regards,
Jozef
Hi Jozef,
The static leakage is given in the datasheet in the electrical characteristics table:
Note that the pins in question do indeed have DACs multiplexed on them, hence the additional leakage current seen.
The other component to consider, while not strictly leakage, is that you will see an average effective in-rush or out-rush current potentially as high as Ch*sample rate. This is due to the internal ADC S+H capacitor, Ch, equalizing with the external driver at the beginning of each sample. Each sample pulls (or pushes) some charge from the pin and when repeated periodically this can appear like a sample-rate dependent leakage current:
Hi Devin,
This information was exactly what I needed. Thank you.
I have to use a Fully-Differential Amplifier to drive ADC in Differential Mode.
Regards,
Jozef
Hi Jozef,
For driving fully differential ADC, you need:
Note also that F2838x family devices are very similar to F2837x family devices, but they also support using 16-bit ADC in single-ended mode (naturally the performance is still better in 16B differential mode).