Part Number: TMS320F28388D
I want to use SCI boot. I'm asking about the boot select pin and SCIA pin settings.
After setting BMSP register, BOOT_DEF register, OTP_BOOTPIN_CONFIG_KEY, etc.
I think I can adjust the boot mode according to the hardware I configured.
However, the question is how to boot the chip with SCI for the first time before setting the register.
Since KEY is not yet 0x5A,
If GPIO84=1, GPIO72=0, it will branch to SCI boot.
TRM says only SCIA ports are available, but it doesn't say which pin to use.
[Figure 5-3. CPU1 Standalone Boot Flow] has no part to check BOOT_DEF when KEY is not 0x5A.
Is it possible with any pin of SCIA? Or is it only possible with the initial values of BOOT_DEF, GPIO29 and GPIO28 pins?