Other Parts Discussed in Thread: LAUNCHXL-F280049C, , C2000WARE, CONTROLSUITE
I have a launchxl-f280049c which I have successfully used to drive a motor using the C2000Ware motor control SDK example project dual_axis_servo_drive_fcl_qep_f28004x. I now want to add a boostxl-posmgr to implement a BISS-C absolute encoder interface. However I cannot find the relevant library functions. In fcl_sensored_pmsm_iddk_users_guide SPRACL1A table 1 lists the FCL interface function FCL_runAbsEncPICtrl(). However this is not in the FCL motor control SDK library users guide and is unresolved when added to the project.