Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am working on using SCI with fiber and I would like to configure the SCI in UART mode.
1. How do I configure the SCI in UART mode ? Are the protocols for UART and multiprocessor modes the same ?
2. How does the idle-line wake up and the address bit wake up make a difference in UART mode ? If I go with the address bit wake up mode, is the address the address of the slave ?
3. In case I disable the sleep bit and the Twake bit and choose idle line mode, do I still have to follow the protocol defined by the idle line multiprocessor mode ?