Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Hello,
I'm trying to help a customer figure out pin muxing for a schematic and wanted to use pinmuxtool/ sysconfig to help with the process, but it seems like the tool is missing pinmux options for the SCI peripheral. For example I'm using the 56 pin RSH package, sysconfig offers me these options for SCIA:
But in the datasheet I see that SCIA_RX can also be muxed to pins, 44, 56, and 31.
Is there something I'm doing wrong, or is there some reason these additional pins don't get reported in syscfg?
Munan