I can't seem to clear the FIFO interrupt flag on the F28035 DSP. I tried clearing the interrupt using the TXFFINTCLR bit on the F2808 DSP and it works fine.
On the F28035, the interrupt flag goes high as soon as the FIFO transmitter is enabled and only goes low when the FIFO transmitter is disabled. TXFFIL doesn't affect this interrupt either.
The RXFFINT works just fine, btw. RXFFINTCLR clears it as it should. Does the TXFFINT operate differently than the RXFFINT? or is there something else I'm missing?
Regards,
Kerson.