Part Number: TMS320F28379D
Hello,
I am looking to synchronize the EPWM modules of two different 28379 DSPs using a synchronization signal from a third 28379 DSP. As per the manual, the best possible solution is to use the EXTSYNCOUT and EXTSYNCIN through the X-bar for synchronization.
1. With the aforementioned approach what should be the width of the pulse that is to be used for synchronization. Does the synchronization work based on the rising edge or the falling edge of the pulse ?
2. Is there an alternate way to do it via eCAP i.e., capture the rising the rising edge of the sync pulse using eCAP and generate an interrupt to reset the EPWM TB counter. Or should the synchronization pulse be generated through eCAP.
3. Is there any other better way to do this to achieve good synchronization without significant delays ?
Thanks & Regards,
Radha