This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
according to my previous post (CCS/LAUNCHXL-F280049C: OTP - common understanding / reprogrammable), I am still unaware, how to actually set the values of
EMU-BOOTPIN-CONFIG / EMU-BOOTDEF-LOW / EMU-BOOTDEF-HIGH instead of their equivalents in OTP (Z1-OTP-BOOTPIN-CONFIG,...).
Could you please explain exactly how I should proceed to set these values to be used in emulation boot mode?
I coud not find anyting in TRM.
Thanks in advance & best regards,
Felix
Felix,
"Table 4-12. Boot ROM Registers" of TRM has address for emulation boot registers and "Table 4-5. BOOTPIN_CONFIG Bit Fields/Table 4-7. BOOTDEF Bit Fields" have definition of these registers. Once you are connected to device via CCS, open the address location in CCS memory watch window and update the value as needed. After setting the values, issue reset from CCS and now when you click on "Run", device will boot as per the emulation boot settings.
Hope this helps.
Regards,
Vivek Singh