This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am Working on the Steering Pump Motor Application.
Need a confirmation that Sensor-less BLDC Motor with InstaSPIN-FOC method is possible or not.
Please provide the Advantages and Disadvantages of the Sensor-less BLDC Motor with InstaSPIN-FOC method.
Here, Sensor-less means that without HALL Sensor Signals(A,B,C) from BLDC Motor, Is my understanding is correct or not.
Thanks,
Krishna.
Sensorless BLDC is typically HALL sensorless. InstaSPIN FOC gives sinusoidal control treating the motor like a PMSM. If you are looking at sinusoidal control instead of 6 step control, this works well. Suitability of sensorless control for the target application is the choice the designer will have to make.
6 step control is audibly noisier, there could be momentary torque ripples, motor size could be bigger for same power, control is easier.
With InstaSPIN-FOC, it is less noisier, minimal torque ripples, higher power output for size, control is complex.