Other Parts Discussed in Thread: TIDM-02008
Good day, I hope you are fine and healthy.
I need to know the Power Losses in the C3M0030090K SiC MOSFET
used for the Full-Bridge Primary & Secondary sides on [TIDM-02002] DC-DC converter
I'm using [TIDM-02008] as the PFC Stage 380-V DC Output @ 3.3-kW.
My Inquiry:
1- Power Losses in the C3M0030090K SiC MOSFET for the Primary & Secondary respectively.
2- Is it possible to use the
C3M0065100K (N-Channel, 1000V, 35A, Rds On (65 mOhm), 113.5W ) instead of
C3M0030090K (N-Channel, 900V, 63A ,Rds On (30 mOhm) , 149W)?
If that possible, what will be the Power Losses in the C3M0065100K SiC MOSFET?
Thanks in advance
Best Regards,
Abdalla Saad