This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
CCS tells me
Description Resource Path Location Type
#6001 cannot open file "C:/ti/C2000Ware_3_02_00_00_Software/driverlib/f2837xd/driverlib": Permission denied emif_ex1_16bit_asram C/C++ Problem
How to get rid of this error?
I put the picture of this project.
Thanks for your help.
---ShunjiKohno
Shunji,
Did you just import the project (C:/ti/c2000/C2000Ware_3_02_00_00/driverlib/f2837xd/examples/cpu1/emif/) or made any changes in the project?
Can you send screen-shot of project explorer?
I imported (C:/ti/c2000/C2000Ware_3_02_00_00/driverlib/f2837xd/examples/cpu1/emif/) and made change a little.
My purpose is using the "rts2800_fpu32_fast_supplement" and "sin_f32" in the "emif_ex1_16bit_asram" project.
This is the Project Explorer screenshots.
Should I show you more details?
Best regards.
Thank you for taking care.
-Shunji
Shunji,
Can you right-click driverlib.lib and check the physical path in property? Does that file exist at that location?
Shunji,
Looks like you have C2000ware 3.02.00.00 and 3.03.00.00 installed and paths are mixed and matched.
Create a fresh workspace and reimport from 3.03 C2000ware driverlib example and try again and do not add Driverlib path manually for both installations.