Part Number: TMS320F28379S
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello, I have to change the CLB code that comes with the t-format master interface, originally with the launchxl-f2839d card, and I want to simulate it as suggested in the clb tool and designing with the c2000 configurable logic block.
The problem is the post-build portion of the build fails.
mkdir "C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation"
makefile:154: recipe for target 'post-build' failed
process_begin: CreateProcess(NULL, ./simulation/simulation_output.exe, ...) failed.
A subdirectory or file C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation already exists.
gmake[1]: [post-build] Error 1 (ignored)
g++: error: Morgan/workspace_v11/PM_tformat_lib: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.d: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o: No such file or directory
g++: error: C:/Users/Don: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg/clb_sim.cpp: No such file or directory
g++: fatal error: no input files
compilation terminated.
gmake[1]: [post-build] Error 1 (ignored)
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/simulation_output.map: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/simulation_output.exe: No such file or directory
g++: error: C:/Users/Don: No such file or directory
g++: error: Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o: No such file or directory
gmake[1]: [post-build] Error 1 (ignored)
gmake[1]: [post-build] Error 2 (ignored)
C:/TDM-GCC-64/bin/g++ -c -DCLB_SIM -IC:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc-2.3.3/src -IC:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/include -IC:/Users/Don Morgan/workspace_v11/PM_tformat_lib -IC:/TDM-GCC-64/bin/include -Og -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MFC:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.d -MTC:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o -IC:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg -fno-threadsafe-statics -oC:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg/clb_sim.cpp
makefile:154: recipe for target 'post-build' failed
C:/TDM-GCC-64/bin/g++ -DCLB_SIM -DF2837xS -Og -g -gdwarf-3 -gstrict-dwarf -Wall -Wl,-Map,C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/simulation_output.map -LC:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc-2.3.3/build/src -oC:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/simulation_output.exe C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/simulation/clb_sim.o C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/src/CLB_FSM_SC_model.o C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/src/CLB_HLC_SC_model.o C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/src/CLB_LUT4_SC_model.o C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/src/CLB_OutputLUT_SC_model.o C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/systemc/src/CLB_counter_SC_model.o -Wl,--start-group -lsystemc -Wl,--end-group
makefile:154: recipe for target 'post-build' failed
./simulation/simulation_output.exe
makefile:154: recipe for target 'post-build' failed
C:/ti/ccs1010/ccs/tools/node/node.exe "C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg/dot_file_libraries/clbDotUtility.js" "C:/ti/c2000/C2000Ware_MotorControl_SDK_3_00_01_00/c2000ware/utilities/clb_tool/clb_syscfg" "C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg" "C:/Users/Don Morgan/workspace_v11/PM_tformat_lib/RELEASE/syscfg/clb.dot"
CLB block diagram SVG was created!
CLB block diagram HTML was created!
I have checked my settings over and over. I get makefile: 154 and makefile: 155 errors.
Everything else works. What do you think?
Thank you, Don