Part Number: C2000-GANG
Other Parts Discussed in Thread: TMS320F28335, UNIFLASH
Hi,
I have C2000 Gang Programmer and want to program TMS320F28335 device. I started "C2000-GANG Programmer" application and connected programmer hardware to the pc over usb. C2000-Gang Programmer application recognized the hardware and PC communication notifications color turned green. I did other settings as shown blow.
firstly I tried to upload .out file which generated by CCS v7 to the target. It did not work. If I upload same file by using UniFlash with XDS110 Debug Probe, it works well. So I program same file with C2000 Gang Programmer and UniFlash and read it back. The image which programmed with C2000 Gang Programmer seems weird as shown blow.
After some research I find a information which mention that I have to use hex2000 utility to generate 16 bit compatible image with -romwidth16 switch. Then I used hex2000 utility and generated s37 image file. This time application runs normally but the device should be csm locked because the image file have csm key programmed with other than 0xFFFF. After I programmed the device with UniFlash, the device locked. Then I used to unlock and program the device with C2000 Gang Programmer but the programmer gave Error:23(MCU init device). By the way I did define the passoword. Do you have any solution?
Thanks in advance.
Best Regards.
Emin ATEŞ