Hello,
is it possible to use the optimization for the CLA compiler? Customer CLA C-code needs a lot of RAM memory. Any hooks to reduce the code size in memory?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
is it possible to use the optimization for the CLA compiler? Customer CLA C-code needs a lot of RAM memory. Any hooks to reduce the code size in memory?
Regards, Holger
HS WG-FAE said:is it possible to use the optimization for the CLA compiler?
Yes. Start by using the build options --opt_level=3 --opt_for_speed=0. Experiment with different values for --opt_for_speed. It accepts the values 0-5.
Thanks and regards,
-George