This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Has there been an update to the 49c lanuch pad PDF ( tSPRUII7A–June 2018–Revised March 2019) to properly indicate booster header pins J6 GPIO pins 14/32, respective EPWM-8A/B? Where is EPWM-7A/B on J6, hal.c has two EPWM8B GPIO noted?
Also there are no PWM-DAC4 GPIO output pin/s defined in SDK 3.01.00.00 hal.c.
So EPWM-8B is configured for GPIO pin 15 but booster header pin map card and schematic both show pin 32, very confusing.
Hi,
Gl said:Has there been an update to the 49c lanuch pad PDF ( tSPRUII7A–June 2018–Revised March 2019) to properly indicate booster header pins J6 GPIO pins 14/32, respective EPWM-8A/B?
Not clear what you're asking about regarding GPIO14/32 on the User / Quick Start Guide.
I'd suggest using the Pinmux tool to identify C2000 signal locations on the LaunchPads.
https://dev.ti.com/sysconfig/?fromPinmux=true#/start
The F28004x LaunchPad does not have PWM DAC signals (i.e. filtered PWMs).
Best,
Kevin