This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am working with LAUNCHXL-F28379D. I have imported i2c_eeprom example code from C2000Ware and run it with the ready available module with EEPROM AT24C32 and RTC DS1307 present on the same module. The code is not working. I have tried to observe the SDA and SCL on oscilloscope but nothing has been observed. I am also tried the same with pull up resistors but again nothing has been observed. I have not made any changes in the example code. I am not getting why this is happened. After doing this I should at least get SCL signal on oscilloscope but this is not happening. Can you please tell me what is the actual problem and what should I do.
Thanks in advance!
Nisha
Nisha,
It is not clear from the above post which I2C EEPROM project you are talking about.
I would encourage you try EEPROM example code available in below path. These example got released recent C2000Ware release.
<C2000Ware>\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex4_eeprom_polling
<C2000Ware>\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex6_eeprom_interrupt
Regards,
Manoj
Manoj,
the following examples are not working:
1) C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2837xd\examples\cpu1\i2c_eeprom
2) C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex2_eeprom
3)C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex3_external_loopback
But the following examples from new version of C2000Ware resolved my issue. They are working fine.
<C2000Ware>\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex4_eeprom_polling
<C2000Ware>\driverlib\f2837xd\examples\cpu1\i2c\i2c_ex6_eeprom_interrupt
Thank You!
Nisha
Manoj,
the following examples are not working:
but the following examples from new release of C2000Ware resolved my issue. They are working fine.
Thank You!
Nisha
Manoj,
Following examples are not working
1) i2c_eeprom from device support->examples->cpu1
2) i2c_ex2_eeprom from driverlib
3) i2c_ex3_external_loopback from driverlib
but the following examples resolved my issue, they are working fine.
1) i2c_ex4_eeprom_polling from driverlib
2) i2c_ex6_eeprom_interrupt from driverlib
Thank You!
Nisha
Nisha,
I shall file a ticket and to check what is wrong with above mentioned code and correct it in next C2000Ware code release.
I'm happy to know below projects resolved your issue.
1) i2c_ex4_eeprom_polling from driverlib
2) i2c_ex6_eeprom_interrupt from driverlib
Regards,
Manoj