Other Parts Discussed in Thread: CONTROLSUITE, TMS320C28346
Routines found on controlSUITE (controlSUITE\device_support\c2834x\v112\DSP2834x_examples_ccsv4), using CCS 9.3 + complier v18.12.4.LTS and CCS 10 + complier v20.2.2.LTS, there is an error when download to the chip, and the error message is "C28xx: Error initializing flash programming: Interface returned from dll, but flash is not available on this device"
The same routine, using CCS 7.4.0 + complier v16.9.6. LTS, can be downloaded to the chip and run normally。
Is it related to the compiler version? Or is it related to the configurations? What should I do? Thank you in advance!