Part Number: TMS320F28388D
Other Parts Discussed in Thread: TPS62420, TMDSCNCD28388D
Dear Ti support team,
I am using MCU: F28388D for my motor control board. Currently I am soldering for the board. I have checked the board before soldering, it seems like there is no problem with the original board.
The sequence soldering belows:
Firstly, I solder parts for power supply block which supplies 3.3V and 1.2V for the MCU. I use the TPS62420DRCR IC for voltage regulator. After finishing, I have checked the output voltage 3.3V and 1.2V, these voltages are Ok (Input : 5V, output 3.3V and 1.2V) .Below is the schematic of power supply block and filter.
Filter for 3.3V and 1.2V:
Next, I continue to solder the F28388D into the board, then I solder the decoupling capacitors for VDDIO, VDDA, VDD, VDDOSC, VDD3VFL pin and VSS - GND around the MCU (all capacitor is 100nF). After finishing, I again check the short circuit between the power pins and VSS - GND pins so everything is still ok , there is no short circuit between power pins and VSS - GND pin. Below is the schematic or MCU supply (I use external crytal 20Mhz for MCU):
Crytal 20Mhz:
Jtag debugger:
Analog supply:
The problem happens when I supply 5V, I see that the MCU get hot and the total consumption current about 0.9A. (about 10s). So I turn off 5V, I realize there is short circuited between 3.3V and GND, so I take 2 ferrarit beams FB2 and FB4 out of the board then check again and see that there is short circuited between VDD_MCU_3.3V (in VDDIO pin) and GND (in VSS Pin), other supply VDD_MCU_1.2V (in VDD pin), VDDA_MCU_3.3V (in VDDA pin), VDD_3.3V (in VDD3VFL) is still normal there is no short circuited.
Finally, I take the soldered MCU chip out of the board:
- Check again pins on the board ,now there is no short between VDD_MCU_3.3V (in VDDIO pin) and GND (in VSS Pin). The power supply (TPS62420) is still working normally, the output 3.3V and 1.2 are still ok.
- I check the pins of the MCU after taking out, It seems like the MCU has died, there is short circuit between VDDIO and VSS pin , the VDD and VDDA, VDDOSC pins are still normal, not get short with VSS pin.
I don't know what I am wrong, can you review the schematic for me or give me the suggestion.
Thanks,
Longpt
.