Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am evaluating the F2837x with the controlCARD R1.1 and C2000Ware_3_03_00_00 examples.
I downloaded the LED blinky example and run.
But it seems to stuck the board.
When I check the suspend button while running, it stops at below line in sysctrl.c
//
// Wait for the SYSPLL lock counter
//
while((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
SYSCTL_SYSPLLSTS_LOCKS) == 0U)
{
;
}