Other Parts Discussed in Thread: MOTORWARE
Hi everyone,
I have purchased a DRV8301-69M-KIT fm TI and a the motor in the link (www.ti.com/.../lvservomtr). I connected the kit to my desktop along with the usb cable. I installed the gui composer, connected all cables originating from the motor to the kit pcb. I supplied 24V & 50V (tried 2 cases) but there was something wrong. After running the gui composer, the motor & kit board were successfully identified.From around 25% to 45% of the motor identification process the motor started revolving smoothly @ 50V/100mA without any weird sounds or anything abnormal. After the identification process reached 100% i clicked on the Tab "Speed or Torque" and later on clicked on the Start/Stop button. After 3-4 seconds the motor started making hiss sounds with its' axis making random clockwise and counterclockwise moves without completing a full revolution. The exact same random behavior (after successfully identifying kit board & motor) occured in both gui composers.
InstaSPIN-FOC & InstaSPIN Motion.
I did not alter any parameters like "Identification Settings" section rectangle, Speed loop tuning PI parameters etc
Can anybody help me go through the process of making the motor revolve with either InstaSPIN-FOC & InstaSPIN Motion?
My motor control knowledge is very basic.
Screenshots provided:
https://snag.gy/2sNGY1.jpg
https://snag.gy/7isfg4.jpg
https://snag.gy/SQbisY.jpg
https://snag.gy/RPhZ2y.jpg
https://snag.gy/lTAGfd.jpg
Regards
Manos Tsachalidis