Other Parts Discussed in Thread: AMC1304M25, AMC1306E25, CONTROLSUITE
Hello,
We purchased the DesignDRIVE Development Kit IDDK v2.2.1 and I have a question on the IDDK_PM_Servo_F2837x project.
With respect to the Delta-sigma modulator device for our application, we are planning to use the AMC1306E25 instead of the AMC1304M25 which is used in the IDDK v2.2.1.
As it is obvious, the output bitstream of the AMC1306E25 is Manchester encoded, whereas the output bitstream of the AMC1304M25 is uncoded.
I have a few questions on the Sigma Delta Initialization routine in the IDDK_PM_Servo_F2837x.c file, when using the AMC1306E25.
(1) With respect to the Input Control Module routine, I may have to apply MODE_2 for the Sdfm_configureInputCtrl function.
(2) Then, with respect to the Comparator module routine and the Sinc filter module routine, can I use the program codes as it is without any modification?
(3) With respect to the Feedbacks OFFSET Calibration Routine, can I use the program codes associated with the SDFM as it is without any modification?
(4) It will be appreciated if some advices are provided to me with respect to developing the program codes when the AMC1306E25 is used.
Thank you for your guidance.
G. Kim