Other Parts Discussed in Thread: DAC8564, CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
I am using CCS8 coding on LAUNCHXL-F28379D to drive DAC8564/5EVM to generate a sine wave.
I can now succefully generate a direct voltage by outputing 24bit data to DAC8564.
But how to generate a sine wave?
I have seen on the page 50 in the document of 'sgen_mdl.pdf' of TI'S controlSUITE the following code.
And I have also seen the struct which defines the paramters which would be used to generate sine wave.
typedef struct {
void (*calc)(void *);
unsigned long int freq;
unsigned long int step_max;
unsigned long int alpha;
int gain;
int offset;
int out;
}SGENHP_1;
(1) However, I did not see the definiton of void (*calc)(void *).
(2) It also said that this function combines loop-up table and linear interpolation method to generate a sine wave. This means I would have to first put a 512 point table( x-> sinx) in the programme memory.
then I define the function which generate sin(x), then I will output this output to the DAC8564 in a 20KHz interrut routine?
(3) As I seen in the datasheet of DAC8564 that the time delay of SPI to DAC out is 10us, then what is the max frequency of sine wave which I could get for DAC8564?
May you give me some idea to generate sine wave?
Thank you!