Other Parts Discussed in Thread: TMDSDOCK28035, DRV8303EVM
Dear team:
I want to use TI example project to drive BLDC motor on TMDSDOCK28035 and DRV8323RH.
I have use the HVBLDC_Sensored project and it worked well. And also does the HVBLDC_Sensorless and InsraSPIN_BLDC with DRV8303EVM.
But when I use the HVBLDC_Sensorless and InsraSPIN_BLDC project on TMDSDOCK28035 and DRV8323RH, it didn't work well. I can see SpeedRpm bouncing a lot in Expressions. The input current of the power supply also fluctuates greatly. This did not happen when using the HVBLDC_Sensored program.
I did not modify the program when using InsraSPIN_BLDC, Because I think the position of the PWM pin and the ADC pin should not be a problem if they are connected correctly.
Is there anything else I should pay attention to?
Do you have a recommended program if I use TMDSDOCK28035 with DRV8323RH?
This is a voltage feedback signal using the sensorless routine, and it is obvious that the front end is abnormal.
Best regards