Part Number: TMS320F28379DZWTT
Hi. whether TMS320F28379DZWTT support Ethernet communication? Does it have inbuilt Ethernet peripheral? if not how to implement it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379DZWTT
Hi. whether TMS320F28379DZWTT support Ethernet communication? Does it have inbuilt Ethernet peripheral? if not how to implement it?
Hi Bharath,
The F2837x family of C2000 devices does not contain an Ethernet peripheral. The full featureset of each of the C2000 devices can be found in each's respective datasheet.
To add Ethernet to a device like one from the F2837x family, you could:
Hopefully this helps!
Thank you,
Brett
Hi Brett,
Thank you for the reply. yes i went through F2838x family mcu. It can be considered for our project. mean while is there any MCU with in built (Emac + Phy) peripheral in TMS320?
Regards,
Bharath
Hi,
In continuation to the previous, It would be good if the MCU is suggested based on the Ethernet stack library which is already available.
Thank you
Hi,
The http://www.ti.com/product/MSP432E401Y has an integrated Ethernet+PHY.
There are also LWIP + FreeRTOS and NDK+TIRTOS stack ports available on that device.
Hope it helps.
Regards,
Sudharsanan
Hi,
Thank you. MSP432 is similar to the one which i am already using TM4C129 with LWIP stack for ethernet communication. But i wanted tms320F2838x family chip with ethernet stack. Main purpose of porting to different chip is for Speed. I want higher cpu speed above 120MHz.
Regards,
Bharath
Hi Bharath,
What is your end application?
As Brett suggested above, will
http://www.ti.com/product/TMS320F28388D
chip from TI serve your need?
Regards,
Sudharsanan
Hi,
my application requires higher cpu speed and with ethernet communication.
TMS320F28388D has Ethernet peripheral but does it come with stack? Can i use lwip stack?
regards,
Bharath
Hi,
Yes. the latest version of C2000WARE http://www.ti.com/tool/C2000WARE
provides a reference LWIP Stack. You can also run TI-RTOS/NDK Stack (if you need an RTOS)
Regards,
Sudhar
Hi,
Glad to know that we could be of help. Thanks for the feedback.
Regards,
Sudhar