Other Parts Discussed in Thread: TCA6424A
Hello,
I am designing a PCB that connects to the TMDSCNCD28379D via the 180pin HSEC connector.
I need more GPIOs than what is available on the HSEC connector, and so I would like to add a port expander, and was looking at using the I2C interface (GPIOs 32 and 33). I am considering using TCA6424A for this to provide additional 24 IOs.
Few questions:
1. Any other recommendation?
2. The SDA and SCL lines, and the INTn signals of the TCA6424A should be pulled up to the Vcc of the host. However the HSEC connector provides no access to the 3.3V generated on the control card. Is it OK to pull up to a local 3.3V that I generate on my own PCB?
3. Is it possible to connect two TCA6424A chips in parallel on the same I2C port - one configured as ADDR=0 and the other as ADDR=1?
4. Is it OK to tie the RESETn of the TCA6424A to the DEVICE_RESET pin on the HSEC connector (this pin is asserted by the TMDSCNCD28379D control card).
Thanks
Uri