Dear team:
1, Does flash-api fuction must run in RAM? If it is not run in RAM, is there any hidden danger?
2, If I call a function B (which do not operate flash) in Function A (which operate flash), Does Function B need to run in RAM?
void FunctionA() { (flash Erase); (flash Read); FunctionB(); (flash write); } void FunctionB() { (No flash operation in it) }
Best reagrds