Part Number: TMS320F280048
Dear Experts,
could You please help with the following questions:
Setup:
On-Board-Charger application
1x F28004x on cold side
1x F28004x on hot side
Needs:
1. high-speed communication for control between uC1 and uC2 (isolated)
2. FW update capabiltiy in the field of both uCs
Questions:
I can only think of the FSI or SPI in high-speed mode configuration.
Is there a way to use FSI for FW update? The boot-mode only supports SPI, so I do not think so. Can You confirm?
Or are there any other ways to get the high communication speed of FSI and FW update capability at the same time over one interface w/o the need for additional isolation devices.
Many thanks and best regards,
Gregor