Tool/software: Code Composer Studio
hello ,
I am using TMS320F28379D controller, currently i have written a boot loader to load motorola S2 record format on the controller for the application file. i am not confident in identifying if the S2 record generated is correct or the BL is incorrect.
i used the hex tool present in bin folder of CCS with following options
Command Line parameters:
${command} ${flags}-m2 ${output_flag} ${output} ../../Tools/s2RecordGenTool/HexConversionOfcCore1.cmd
HexConversionOfcCore1.cmd: contains
F28379D.out
-image
-memwidth 16
ROMS
{
EPROM1: org = 0x088000, len = 0x017FFD, romwidth = 16,
fill = 0xFFFF,
files = { OfsCore1.s2 }
}
I would like to know if Ti has any tool which can load S2 record on F28379D so that i can verify to confirm my S2 record is correct.
Thanks,
Nagesh