Hi,
We're trying to identify an ACIM motor at our university.
We have custom hardware.
We have worked through the InstaSpin labs, everything works perfectly with a PM motor.
Now we're trying an ACIM motor that starts with Lab_2b but we don't have much information about it. Just the following:
Voltage: 42V
Power: 48W
Speed: 2600
The problem now is that the identification process stops after/while Rated Flux and then changes to CTRL_State_Error
I attached our user.h file copied from user_j1.h boostxl8301 project customsettings.h