This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379S: TMS320F28379SZWTT

Part Number: TMS320F28379S

Configuring the SPI-C port under GPIO index 6, assigns SPISIMOC (I/O) to GIO50, GPIO100 & GPIO122. How do i determine which ball of the microcontoller the signal will be routed. I need it to be routed to ball T8

  • Hi John,

    The mux configuration is for each GPIO pin and not for the function, This mean user will configure the mux setting for GPIO100 or for GPIO50 (or any other GPIO) to choose SPISIMOC function. User need to choose only one GPIO for a specific function and should not use multiple GPIO for same function.

    Hope this helps.

    Regards,

    Vivek Singh