This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello dear,
I am designing SMSP with power factor correction. The reference design is based on UCC28600 120-W Evaluation board. The power factor correction outputs upto 390V. I am looking for a transformer replacement for the one used for the UCC28600 section, that is, the FA2443-ALC manufactured by Coil. The transformer category used is signal transformer, is this different from flyback transformer? Also, concerning the input range, most SMSP transformers primary input are rated 85-265 VAC, can this be used for the 390V from the output of the power factor correction to the input of the transformer used in UCC28600? In other words, do you have any recommended cost effective transformer that can be used instead of FA2443-ALC? Input range upto 390V, Output 19-24VDC, 5-6A
Kind regards,
Bright
Hi Mr. Bright,
Thank you for reaching out on UCC28600.
I see that the transformer belongs to category of power transformer as seen in screenshot below.
Unfortunately, I have checked most reference designs, but there is no design wich exactly matches the requirement listed here like the power level or voltage range. So it will probably need to be customized by Wurth electronics or coilcraft.
If you see the EVM waveforms, you should be able to run it at 390V easily.
The Vds is 200V/div, signifying the input voltage of around 400V (output of PFC stage).
Regards,
Harish
Thank you for the reply. Just to confirm, I can use 390 VDC input on flyback transformers rated 85-265VAC at the primary section?
Kind regards,
Bright
Hi Robert,
Yes, the input to flyback stage is around 390V as it is the PFC output. So it should be ok to hook up this voltage to the input of flyback stage.
Thank you
Regards,
Harish