Other Parts Discussed in Thread: TMS320F28069, C2000WARE
Tool/software: Code Composer Studio
Hello all,
I have the following setup:
TMDSDOCK28069 Experimenter hardware Kit and CCS V8.1
I have imported an example project which builds fine with latest C2000 compiler toolchain
The supplied USB .cable is attached to the experimenter kit hardwrae.
The board switch is set to USB.
When I try to debug the application i get the following errors:
C28xx: Error occurred during flash operation: Cannot read 0x00000882@Data: data is not present.
C28xx: Flash Programmer: Warning: The configured device (TMS320F28069), does not match the detected device ().
When I look at Project->properties->CCS General, I see that the linker command file is: 28069_RAM_lnk.cmd??
How to get a 28069_Flash_lnk.cmd?
Any help I from you folks I will appreciate!
Tnaks
Max