Hi,
There is no 28377S examples in the resource explorer. and for other devices the directory is empty.
thanks vadim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There is no 28377S examples in the resource explorer. and for other devices the directory is empty.
thanks vadim
Vadim,
Can you see the examples in F28377D? You can use those examples in CPU1 folder.
Hi Santosh,
Thank you for your help!. I have this error
error connecting to the target:
(Error -1156 @ 0x0)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
I tested connection and it is fine.
How can I paste images and code to the post? I was able to do it in the past.
thanks vadim
Just copy the file in clipboard and paste it in the edit box. It should attach the video, image file.
Thank you!
MEMORY { PAGE 0 : /* Program Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */ /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x000123, length = 0x0002DD RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002Much easier than used to be!
How can I insert the code to keep color?
I do not think there is a way to keep code in color.
We can select the language in code insert, and I think it formats accordingly. I am pasting C code to test here, please ignore the code.
// // Wait to be sure that this interface is not busy. // while((HWREGH(base + CAN_O_IF1CMD) & CAN_IF1CMD_BUSY) == CAN_IF1CMD_BUSY) { }
I will check internally if there is a way and will let you know.